百度翻译为; 定义缺少参数名称[=值]” 这个到底怎么搞啊/
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
#ifndef TARGET_IS_BLIZZARD_RB1
#define TARGET_IS_BLIZZARD_RB1
#endif
#include"stdint.h"
#include"stdbool.h"
#include"LCDDriver.h
" #include"LCDDriver.c"
#include"inc/hw_memmap.h"
#include "driverlib/rom.h" #include "driverlib/rom.h
" #include"inc/hw_ints.h"
#include "driverlib/interrupt.h"
#include "inc/hw_gpio.h"
#include "MenuFrame.h"
#include "math.h"
#include "MenuFrame.c"
#include"TestConfig.c"
#define PERIOD_TIME 12500 / 20
#define ADC_BASE ADC0_BASE // 使用ADC0
#define SequenceNum 3 // 使用序列3
void Init_LCD_Show() {
// 使能LCD LCD_Enable();
// 初始化LCD LCD_Init();
// 初始化LCD屏做清屏工作 LCD_ScreenClr();
}
int main(void){
{
Init_LCD_Show();
Init_Test_DCDC_Boost();
}
while(1) {
unsigned long ADC_ValueGet(uint32_t ui32Base, uint32_t ui32SequenceNum); Handler_ADCWheel(); Handler_Test_DCDC_Boost();
Refresh_LCDView();
} }
LCD不显示电压电流值