This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4c1294修改BOOTCFG寄存器导致程序无法运行问题,怪!

Other Parts Discussed in Thread: EK-TM4C1294XL, EK-TM4C123GXL

1  测试平台:EK-TM4C1294XL ,    ARM型号:XM4C1294NCPDT。

2  目的:设置BOOTCFG寄存器,使的PA6引脚上电低电平时使得ARM进入ROM中的bootloader。

3 测试程序:利用例程blinky,在其中添加设置BOOTCFG寄存器代码如下:

void CheckBootCfg(void)

{

    long i=0;  

    unsigned long regVal;  

   regVal = HWREG(FLASH_BOOTCFG);

    if(regVal & FLASH_BOOTCFG_NW)

   {   

           HWREG(FLASH_FMA) = 0x75100000;         

          regVal = FLASH_BOOTCFG_PORT_A | FLASH_BOOTCFG_PIN_6 | FLASH_BOOTCFG_KEY | FLASH_BOOTCFG_DBG1;

          HWREG(FLASH_FMD) = regVal;

          regVal = FLASH_FMC_WRKEY | FLASH_FMC_COMT;   

          HWREG(FLASH_FMC) = regVal;

         while((HWREG(FLASH_FMC) & FLASH_FMC_COMT) == FLASH_FMC_COMT)   {  }

    }

}

4 现象:程序下载后,如果系统上电时,PA6引脚处于低电平,通过连接USB到电脑,观察设备管理器出现的USB DFU设备,确认ARM进入ROM中的bootloader;

                                    如果系统上电时,PA6引脚处于高电平,此时电脑设备管理器并未出现USB DFU设备,可推断ARM并未进入ROM中的bootloader,此时应该进入flash中的blinky程序,闪烁lED,但事实是ARM无任何动作,并未运行blinky程序。

 

5 问题总结:通过PA6引脚低电平可控制ARM进入ROM中的bootloader,但当PA6上电处于高电平时,ARM无法正常加载flash中的用户程序运行。

 

经过多次测试,问题依然如此,请TI工程师帮忙分析一下原因。