This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
近期MCU(微控制器)市场可能又要出现涟漪了,尽管ARM推出新款的处理器核心Cortex-M7,不过TI(德州仪器)在Cortex-M4领域,有更多的期待与想法,所以依Cortex-M4为主体,在既有的MSP430产品架构上,又开辟出一条全新的MSP432系列。
TI科技委员会委员暨嵌入式系统总监詹勋琪表示,过去MSP430主打低功耗与低成本路线,但我们也发现,即便有这样的诉求,客户也很在意性能表现,所以把Cortex-M4作为MSP432的处理器核心。其最大的操作时脉可达48MHz,可以动态调整时脉高低,采用90奈米制程。詹勋琪直言,单单采用Cortex-M4,是无法与其他竞争对手形成差异化,以性能表现为例,在经过评测后,其Coremark score为3.41/MHz,这与其他对手的产品相较,并没有太大的差异。TI的作法并不是只将处理器核心搬进MCU而已,而是针对整个MCU系统进行客制化。
首先,TI从功耗方面下手,MSP432内部整合了LDO与DC/DC转换器,这也是市场上少数整合了DC/DC转换器的MCU产品,在操作电压方面,其范围为1.62至3.7V,在主动模式下可以达到95μA/MHz,睡眠模式(在震荡器工作状态下)的消耗电流为850nA,詹勋琪不讳言,会推出这样的产品线,就是锁定了同样都是采用Cortex-M4架构,但还未成为TI的客户群,因为市场上的Cortex-M4架构的MCU的功耗表现还是不尽人意。
TI科技委员会委员暨嵌入式系统总监詹勋琪(摄影:姚嘉洋)
至于原有的MSP430产品线,TI接下来会以FRAM(铁电随机存取记忆体)为主的产品线作为主力,毕竟FRAM在读写次数上远胜其他现有的记忆体种类,有很多应用方面,都很需要这类产品线的奥援。所以MSP430与MSP432各有其市场区隔,不会产生竞争关系。而原先采用MSP430的客户群,也能很容易地将设计移植到新款的MSP432上。
更多信息可以参考 http://www.deyisupport.com/question_answer/w/faq/526.msp432-faq.aspx?keyMatch=MSP432&tisearch=Search-CN-Support