This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

死亡来临?当MSP430遭遇MSP432



 MSP430 MCU世界里的一则神话, 全球16位MCU最低功耗的标杆,过去20年来从未被超越,是工程师眼中当之无愧的低功耗之王。近日,TI隆重推出了基于ARM Cortex-M4F内核的32位低功耗MCU产品——MSP432。

 

1.jpg

 

这一功耗更低、性能更佳的MCU产品家族的诞生,是否会打破MSP430低功耗之王的神话?答案揭晓前,让我们先对二者进行一下比较。

 

2.jpg

 

通过上表可以很明显地发现,MSP430和MSP432在产品定位和应用优势上是不一样的。两者并不存在竞争关系,MSP432的出现不仅不会取代MSP430,反而将TI低功耗MCU的理念与优势从16位领域延伸至32位领域。

 

0.jpg

“低功耗MCU是TI业务中很重要的组成部分,目前,我们可以向客户提供超过500款的低功耗MCU产品。无论是16位产品还是32位产品,我们都将持续投入下去。” TI副总裁兼微控制器事业部总经理Ray Upton。

 

 

4.jpg

 

功耗or性能?抓狂!

一直以来,开发人员在功耗和性能之间不断做着妥协与权衡,无奈之下只能二选一,要么牺牲一部分性能以降低功耗,要么提升功耗以满足高性能需求。可是越来越多的应用同时提出了高性能和低功耗的设计要求,开发人员面对如此两难的选择头痛不已。

 

0.png

 

“MSP432用与M0+相近的功耗实现了Cortex-M4F的性能,让开发人员同时获得超低功耗和最佳性能,无需做出任何妥协。”TI超低功耗MSP微控制器事业部总经理Miller Adair。

Why?最低功耗

 

6.jpg

 

 

7.jpg

 

Why?最佳性能

 

8.jpg

 

 

9.jpg

 

MSP430与MSP432:一脉相承

从两个产品系列的命名规则可以看出,二者同属于TI低功耗MCU产品组合,MSP432在产品设计和产品理念上都是MSP430的一种延续。MSP432平台汇集了TI过去20年间设计MSP430的各种经验和IP成果。

而且,因为MSP430和MSP432采用相同的API驱动,二者的代码、寄存器及低功耗外设是兼容的,所以客户的软件设计可以在MSP430和MSP432之间无缝移植。

综上,MSP432的问世,并没有威胁MSP430在16位MCU领域低功耗之王的地位,反而将TI在超低功耗的领先地位延伸至32位MCU领域。通过MSP430和MSP432的可扩展产品组合,TI的客户可以根据应用领域和设计需求选择最合适的MCU产品,在不影响用户体验的情况下集成更多的功能。