This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tm4c123gxl的串口uart0和uart3的问题



uart0可以正常收发,但是uart3发送的时候碰到延时函数会挂在那,没碰到还可以发送,并且为什么接收也不行


#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "driverlib/debug.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"


#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif


signed int GsmRcv[50];
uint8_t GsmAtFlag = 0;
uint8_t GsmRcvCnt = 0;


//*****************************************************************************
//
// The UART interrupt handler.
//
//*****************************************************************************
void
UARTIntHandler(void)
{
uint32_t ui32Status;

ui32Status = ROM_UARTIntStatus(UART3_BASE, true);
// ui32Status = ROM_UARTIntStatus(UART0_BASE, true);

//ROM_UARTIntClear(UART0_BASE, ui32Status);
ROM_UARTIntClear(UART3_BASE, ui32Status);

GsmRcvCnt = 0;

// while(ROM_UARTCharsAvail(UART0_BASE))
while(ROM_UARTCharsAvail(UART3_BASE))
{
//GsmRcv[GsmRcvCnt]=ROM_UARTCharGetNonBlocking(UART0_BASE);
GsmRcv[GsmRcvCnt]=ROM_UARTCharGetNonBlocking(UART3_BASE);

// ROM_UARTCharPutNonBlocking(UART0_BASE,
ROM_UARTCharPutNonBlocking(UART3_BASE,
                                GsmRcv[GsmRcvCnt]);
GsmRcvCnt++;

GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, GPIO_PIN_2);

SysCtlDelay(SysCtlClockGet() / (1000 * 3));

GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, 0);

}
}
//·¢ËÍ×Ö·û
void Uart1Send(uint8_t c)
{
//UARTCharPut(UART0_BASE, c);
UARTCharPut(UART3_BASE, c);
}

//·¢ËÍ×Ö·û´®
void Uart1Sends(uint8_t *str)
{
while(*str!='\0')
{
Uart1Send(*(str++));
}
}
//ÑÓʱ
void DelaySec(uint32_t sec)
{
uint32_t i , j= 0;

for(i=0; i<sec; i++)
{
for(j=0; j<65535; j++)
{
}
}
}
//Çå³ýÊÕµ½µÄµÄÊý¾Ý
void initGsmRcv()
{
for(int i=0;i<50;i++)
{
GsmRcv[i]='0';
}
}
void tcptest()
{


Uart1Sends("AT+CGCLASS=\"B\"\r\n");
DelaySec(300);
Uart1Sends("AT+CGDCONT=1,\"IP\",\"CMNET\"\r\n");
DelaySec(300);
Uart1Sends("AT+CGATT=1\r\n");
DelaySec(300);
Uart1Sends("AT+CIPCSGP=1,\"CMNET\"\r\n");


DelaySec(300);
Uart1Sends("AT+CLPORT=\"TCP\",\"2022\"\r\n");
DelaySec(300);
Uart1Sends("AT+CIPSTART=\"TCP\",\"103.44.145.243\",\"32154\"\r\n");
DelaySec(1000);
Uart1Sends("AT+CIPSEND\r\n");
DelaySec(300);
DelaySec(300);
Uart1Sends("DANGEROUS");
DelaySec(300);
Uart1Send(0x1a);
DelaySec(1000);
DelaySec(300);
Uart1Sends("AT+CIPCLOSE\r\n");
DelaySec(300);
Uart1Sends("AT+CIPSHUT\r\n");
DelaySec(300);
}


int
main(void)
{
ROM_FPUEnable();
ROM_FPULazyStackingEnable();

ROM_SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_16MHZ);

ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);

ROM_GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_2);


// ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
// ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART3);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);

ROM_IntMasterEnable();

//GPIOPinConfigure(GPIO_PA0_U0RX);
//GPIOPinConfigure(GPIO_PA1_U0TX);
//ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
GPIOPinConfigure(GPIO_PC6_U3RX);
GPIOPinConfigure(GPIO_PC7_U3TX);
ROM_GPIOPinTypeUART(GPIO_PORTC_BASE, GPIO_PIN_6 | GPIO_PIN_7);

//ROM_UARTConfigSetExpClk(UART0_BASE, ROM_SysCtlClockGet(), 115200,

ROM_UARTConfigSetExpClk(UART3_BASE, ROM_SysCtlClockGet(), 115200,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE));


// ROM_IntEnable(INT_UART0);
// ROM_UARTIntEnable(UART0_BASE, UART_INT_RX | UART_INT_RT);
ROM_IntEnable(INT_UART3);
ROM_UARTIntEnable(UART3_BASE, UART_INT_RX | UART_INT_RT);


//×Ô¼ºµÄº¯Êý
tcptest();
}