This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在升级为win10之后ccs安装时总是出现问题:your installer source path contains non-ascll chararters which can corrupt the installation 。请问如何解决该问题?
Check your source path; there seems to be an issue. Can you paste the directory address where you're installing CCS.
Also, make sure that the path contains no spaces by looking up the file-system.
去官网下载最新版,如果你的网速可以也可以用在线安装版本。目前是Code Composer Studio 6.1.2
我就是在WIN10下选择的在线安装版本,非常好用。前提是网速很快才行。我的网速还可以
请问CCS3 .3能够在win10 professional下运行安装吗?
由于现在开发的板子TMS320DM6467的开发板SEED-DVS6467教程使用的是CCS3.3,现在电脑上装的是CCS6.1.1,Debug的时候能运行,但是点击其他按钮是整个程序就无响应了,也不知道是什么问题,想换个版本试试,还有就是是不是CCS6.1.3以上才很好的支持win10吗?或者我换成CCS6.1.3试验一下?
CCS6是可以在win10上使用的,CCS3.3基本就没有希望了
好的,谢谢您的回复,我再试试CCS6.1.3吧,不行的话我就换台电脑操作吧!
不可以,请使用最新版在Win10下运行。。6之前的版本都不行。。6早期的版本好像也不行。。