This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-MSPM0L1306: MSPM0G3519-Q1

Part Number: LP-MSPM0L1306
Other Parts Discussed in Thread: MSPM0G3519-Q1

你好!我们现在采用MSPM0G3519-Q1做HUD产品的主控芯片,有如下问题请回复下,谢谢!

1,MSPM0G3519-Q1 MCU有几路CAN接口?规格书上IO 定义有写是两路,但是介绍资料又是写成一路。

2,MCU MSPM0G3519-Q1ADC检测最小电流是多少?

3,DRV8889QWRGERQ1的VREF可否通MCU MSPM0G3519-Q1的DAC脚输出控制输出电流?

4,MSPM0G3519-Q1有2 个 4Msps 12 位 ADC,但每个ADC分10几个PIN脚,是否这些PIN脚可同时使用?如何分批采用?

5,MSPM0G3519-Q1 HFX晶体要求范围是4M-48MHZ,选用24MHz有没有问题?

6,MSPM0G3519-Q1 LFX的晶体 32.768KHZ,如果没有RTC要求是否可取消?

7,SPI信号一般的叫法是MISO也可以是SIMO,DOUT,DO,SDO或SO,MOSI也可以是SOMI,DIN,DI,SDI或SI  MSPM0G3519-Q1 MCU SPI_PICO是对应MOSI还是SIMO?