This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1294KCPDT: 技术咨询

Part Number: TM4C1294KCPDT

你好,    

     在使用该芯片的过程中我们发现SPI的MOSI线在idle状态下,会有异常的电压抬升,详细可见下图:

该路(SSI0)SPI用于驱动SD卡,配置为2MHz(1M和500kHz的情况下,该问题也还是存在)IO初始化配置如下所示:

如下为硬件设计原理图,在排查测试中拆除过D1g/C2g-C5g都还是存在该问题。其中SPI通讯线上拉电阻为10K。

基于上述情况,请帮忙分析一下是什么原因导致的,谢谢!