This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL132EZWTA2



OMAPL132EZWTA2 Same software with external circuitry (hardware problematic and non-problematic external crystal oscillator (crystal frequency: 19.2MHZ) no difference, the circuit design on the PCBA board is the same) After starting up and running, the internal timer of the chip sends out the wrong signal, using 1500 pieces, it is found that 40 pieces of the internal timer of the chip sends out the wrong signal.

  • 您好

    我们建议您请按照以下方式联系客户支持部门,会有客服为您提供帮助。
    打开链接ticsc.service-now.com/csm
    点击“申请新的支持”下面的“提交申请”按钮
    在新打开的窗口中点击“质量,可靠性和环境信息”下面的“创建案例”按钮
    在打开的表格中您可以使用中文描述您的问题并且递交。
    会有专员为您服务。