MSPM0G3507做为IIC从机,主机进行数据读取出现问题,我这边I2C协议的头数据应该为EE,但是在极低概率(300次可能出现1-2次)中读取的头字节变为了00,第二个字节变成了EE,通过逻辑分析仪抓取的数据如下:
应该如何解决?
正常数据:

异常数据:

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
MSPM0G3507做为IIC从机,主机进行数据读取出现问题,我这边I2C协议的头数据应该为EE,但是在极低概率(300次可能出现1-2次)中读取的头字节变为了00,第二个字节变成了EE,通过逻辑分析仪抓取的数据如下:
应该如何解决?
正常数据:

异常数据:

您好
当您在使用MSPM0G3507作为I2C从机时,遇到主机读取数据出现头字节错误(预期为EE,但偶尔变为00,且第二个字节变为EE)的问题,这可能是由于多种原因导致的。以下是一些可能的原因和相应的解决方案:
I2C总线干扰或噪声:
MSPM0G3507配置错误:
主机发送的起始信号或停止信号不稳定:
MSPM0G3507内部故障: