This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0L1106: 如何灵活定义一次timer 中断时间

Part Number: MSPM0L1106


uint32_t timer1_int=0;
void TIMER_1_INST_IRQHandler(void)
{
    timer1_int = DL_TimerG_getPendingInterrupt(TIMER_1_INST);
    DL_TimerG_clearInterruptStatus(TIMER_1_INST,DL_TIMER_IIDX_CC0_UP);
    if(timer1_int == DL_TIMER_IIDX_CC0_UP)
    {
         DL_TimerG_stopCounter(TIMER_1_INST);
         DL_Timer_setLoadValue(TIMER_1_INST,10000);
         DL_GPIO_togglePins(GPIO_PORT,GPIO_ON_OFF_PIN);
         DL_TimerG_startCounter(TIMER_1_INST);
    }
}
这个定时中断可以周期进入,我想写一个接口可以修改为1ms 为base ,可以有参数配置为3ms,5ms 等,我没找到 用哪个API 可以清除TIMER 的值,和配置比较值来调整时间中断