This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TM4C1294NCPD的IO口除USB外哪些能耐5V,串口能耐5V吗?
耐心找了一下datasheet,在文档中找到了答案,就不删帖了,我自己来回答下,帮助更多的人解决疑惑。
在Tiva™ TM4C1294NCPDT Microcontroller DATA SHEET中第27章中有以下说明:
除了USB的USB0VBUS(PB1)外,所有IO口都只耐3.3V
可以耐5V
你那个应该不对,应该是配置为输入的时候,除几个引脚可以最高承受3.6V的电压的时候,其他引脚都可以承受5V的电压。不然,5V的信号,进来怎么办,不至于所有的外设都必须3.3v供电吧。
沒錯..我自己正在用這顆, 所有"輸入"到GPIO腳, 都要3.3V, 外設有5V的, 都要用Level shift 降到3.3V.
GPIO輸出3.3V給外設5V的, 就沒差了, 還是一樣當High Level.
我的意思是,5V的外设输入到3.3V的,你可以加3.3V的上拉。3.3V输出到5V的,你可以直接驱动,或者加5V上拉都可以