使用TM4C123GH6PZ开发产品用C语言和ARM汇编语言怎么做呢,具做就是程序主体有C语言去实现,部分功能要用到ARM汇编语言实现,我找了一些方法,在KEIL5.17下编译总是报错。以前做过51单片机的混编,是可以实现的,实在用ARM芯片,不知道片么做了,请大侠指点。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用TM4C123GH6PZ开发产品用C语言和ARM汇编语言怎么做呢,具做就是程序主体有C语言去实现,部分功能要用到ARM汇编语言实现,我找了一些方法,在KEIL5.17下编译总是报错。以前做过51单片机的混编,是可以实现的,实在用ARM芯片,不知道片么做了,请大侠指点。
这个是在MDK环境下的代码。其他的也大概类似。
#if defined(ewarm) || defined(DOXYGEN)
void
SysCtlDelay(uint32_t ui32Count)
{
__asm(" subs r0, #1\n"
" bne.n SysCtlDelay\n"
" bx lr");
}
#endif
#if defined(codered) || defined(gcc) || defined(sourcerygxx)
void __attribute__((naked))
SysCtlDelay(uint32_t ui32Count)
{
__asm(" subs r0, #1\n"
" bne SysCtlDelay\n"
" bx lr");
}
#endif
#if defined(rvmdk) || defined(__ARMCC_VERSION)
__asm void
SysCtlDelay(uint32_t ui32Count)
{
subs r0, #1;
bne SysCtlDelay;
bx lr;
}
#endif
//