我用的TM4C123GH6PM,Tiva C LanunchPad。
写程序,可是一运行到下面这句,
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART1);
程序就跑飞了。
这是怎么回事呢?
我查了一下,串口1 U1Rx这个脚还有模拟功能USB0ID,U1Tx这个脚还有USB0VBUS的功能。
是不是这个复用了?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用的TM4C123GH6PM,Tiva C LanunchPad。
写程序,可是一运行到下面这句,
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART1);
程序就跑飞了。
这是怎么回事呢?
我查了一下,串口1 U1Rx这个脚还有模拟功能USB0ID,U1Tx这个脚还有USB0VBUS的功能。
是不是这个复用了?谢谢!
不对呀,不是这个语句的问题,我同样用的是Tiva C LanunchPad,开头使用了这个语句,没有跑飞的现象
//*****************************************************************************
//
// hello.c - Simple hello world example.
//
// Copyright (c) 2012-2014 Texas Instruments Incorporated. All rights reserved.
// Software License Agreement
//
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
//
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
//
// This is part of revision 2.1.0.12573 of the EK-TM4C123GXL Firmware Package.
//
//*****************************************************************************
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/debug.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
//#include "utils/uartstdio.h"
//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>Hello World (hello)</h1>
//!
//! A very simple ``hello world'' example. It simply displays ``Hello World!''
//! on the UART and is a starting point for more complicated applications.
//!
//! UART0, connected to the Virtual Serial Port and running at
//! 115,200, 8-N-1, is used to display messages from this application.
//
//*****************************************************************************
//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif
////*****************************************************************************
////
//// Configure the UART and its pins. This must be called before UARTprintf().
////
////*****************************************************************************
//void
//ConfigureUART(void)
//{
// //
// // Enable the GPIO Peripheral used by the UART.
// //
// ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
// //
// // Enable UART0
// //
// ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
// //
// // Configure GPIO Pins for UART mode.
// //
// ROM_GPIOPinConfigure(GPIO_PA0_U0RX);
// ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
// ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
// //
// // Use the internal 16MHz oscillator as the UART clock source.
// //
// UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
// //
// // Initialize the UART for console I/O.
// //
// UARTStdioConfig(0, 115200, 16000000);
//}
//*****************************************************************************
//
// Print "Hello World!" to the UART on the evaluation board.
//
//*****************************************************************************
int
main(void)
{
//volatile uint32_t ui32Loop;
//
// Enable lazy stacking for interrupt handlers. This allows floating-point
// instructions to be used within interrupt handlers, but at the expense of
// extra stack usage.
//
ROM_FPULazyStackingEnable();
//
// Set the clocking to run directly from the crystal.
//
ROM_SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ |
SYSCTL_OSC_MAIN);
//
// Enable the GPIO port that is used for the on-board LED.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART1);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
//
// Enable the GPIO pins for the LED (PF2 & PF3).
//
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_2);
//
// Initialize the UART.
//
// ConfigureUART();
// //
// // Hello!
// //
// UARTprintf("Hello, world!\n");
//
// We are finished. Hang around doing nothing.
//
while(1)
{
//
// Turn on the BLUE LED.
//
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, GPIO_PIN_2);
//
// Delay for a bit.
//
SysCtlDelay(SysCtlClockGet() / 10 / 3);
//
// Turn off the BLUE LED.
//
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, 0);
//
// Delay for a bit.
//
SysCtlDelay(SysCtlClockGet() / 10 / 3);
}
}