Other Parts Discussed in Thread: CC1352P7, MSPM0L1306
当前我在CC1352P7-1上使用ns_br_FreeRTOS案例,已经跑通了ti-wisunfan-pyspinel和wfantund这两个程序,并且可以正确建立Wi-SUN网络连接。
我发现MSPM0这个开发板可以使用DALI相关的案例,我也下载了MSPM0的SDK,并查看了一下demo。
我想实现这样一个流程:CC1352P7-1 -> MSPM0 -> Mikroe DALI 2 CLICK -> Dali 2 D4i驱动,以获取到驱动的相关数据
但是我目前并没有购买MSPM0这块开发板。
因此先通过CC1352P7-1进行测试,通过自定义DALI相关的一些代码来实现,结果代码成功烧录到开发板,但是Wi-SUN设备无法启动了,似乎是因为内存不足的原因?
请问能否将CC1352P7-1与MSPM0进行连接,并且在CC1352P7上烧录一些自定义的代码,以获取到D4i驱动相关的数据?