This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc1110的RSSI怎么使用?

Other Parts Discussed in Thread: CC1101

在使用CC1110作无线收发时,近距离无法接收信号,想根据RSSI信号控制接收信号,避免阻塞。

  • Hi Niliu,

       近距离无法接收的问题请参考一篇app note swra147。Close-in Reception with CC1101

       CC1110都是类似的。Workaround 2可能是你想要的答案

        

  • RSSI(Received Signal Strength Indicator)是接收信号的强度指示,它的实现是在反向通道基带接收滤波器之后进行的。 为了获取反向信号的特征,在RSSI的具体实现中做了如下处理:在104us内进行基带IQ功率积分得到RSSI的瞬时值,即RSSI(瞬时)=sum(I^2+Q^2);然后在约1秒内对8192个RSSI的瞬时值进行平均得到RSSI的平均值,即RSSI(平均)=sum(RSSI(瞬时))/8192,同时给出1秒内RSSI瞬时值的最大值和RSSI瞬时值大于某一门限时的比率(RSSI瞬时值大于某一门限的个数/8192)。由于 RSSI是通过在数字域进行功率积分而后反推到天线口得到的,反向通道信号传输特性的不一致会影响RSSI的精度。 在空载下看RSSI的平均值是判断干扰的最主要手段。对于新开局,用户很少,空载下的RSSI电平一般小于-105dBm。在业务存在的情况下,有多个业务时RSSI平均值一般不会超过-95dBm。从接收质量FER上也可以参考判断是否有干扰存在。通过以发现是否存在越区覆盖而造成干扰,也可以从 Ec/Io与手机接收功率来判断是否有干扰。对于外界干扰,通过频谱仪分析进一步查出是否存在干扰源。

  • 距离太近,信号会饱和