我的应用场景是,采用DRV8316T以六步换相的方式驱动一台小型BLDC电机,电机线电阻约为1.5欧,两对极,额定转速为三万RPM,供电采用2S电池,供电电压范围为6.0V-8.4V;其余设置情况:采用不带电流限制的6XPWM模式;压摆率选200V每微妙;过流值设为16A,ASR和AAR禁用;控制芯片选用的STM32F405,芯片用8316T的BUCK电路提供3.3V的供电;程序方面,用外部中断的方式检测霍尔值跳变并在中断回调函数中进行换相,换相采用下管常开,上管PWM调制的方式,每次换相先关四个桥臂,再开两个桥臂;在应用过程中,发现供电电压影响运行情况,供电电压在6.0-6.5V范围内,换向过程会导致芯片的3.3V供电跌落,进而导致芯片断电,换相失败,电机失控。电压高于6.5V时则换向正常,不会有3.3V芯片供电电压跌落的情况发生。怀疑是MOS上下管直通导致8316触发了过流保护,进而切断了3.3V供电;但是程序中每次换向都是先关四个桥臂,再开两个桥臂,理论上不会存在上下管直通的情况,在换相程序中,将关管后加入了1-4us延时,再开管,仍然出现电压跌落的现象。因此判断,3.3V电压跌落(8316触发故障保护)的情况,只与外部供电电压有关,但是6-6.5V的供电电压仍在8316允许的供电范围内,为什么会出现这种情况,保护可能是什么触发的?应该怎么解决?