你好:
我们在使用8899时,如果开启负载检测,在没有拔掉电机的情况或者电机没有工作的情况下 也后读到开路故障,请问如果才能正常读取到开路负载故障;即拔掉电机才能读取到开路故障。其他情况下 不能误报开路故障。谢谢。
Hello:
When using 8899, if load detection is enabled and an open circuit fault is detected even without unplugging the motor or the motor not working, may I ask if it is necessary to read the open circuit load fault normally; Only by unplugging the motor can the open circuit fault be detected. In other cases, open circuit faults cannot be falsely reported. thank you.