This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC14131-Q1: 或者这个系列其他的物料,能否通过几片芯片组合实现一个这样的电源,双路输出,正输出+15~25输出可调,负输出-10~-2输出可调的电源。PCB尽可能保持不变,可以通过替换物料实现。多谢啦,我们想做一个标准的SiC的驱动与测试板子,现在每家驱动电压要求都不一样,我们把打算把电源改成可调的。

Part Number: UCC14131-Q1

UCC14131或者这个系列其他的物料,能否通过几片芯片组合实现一个这样的电源,双路输出,正输出+15~25输出可调,负输出-10~-2输出可调的电源。PCB尽可能保持不变,可以通过替换物料实现。多谢啦,我们想做一个标准的SiC的驱动与测试板子,现在每家驱动电压要求都不一样,我们把打算把电源改成可调的。多谢!

  • 您好,

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待

  • 是的,UCC14/5x系列中的所有IIB(集成隔离偏置)MV(中压)变体都兼容p-2-p。但是,您需要注意输入/输出电压差,当您更改输出电压设置时,为了满足不同栅极驱动电压的要求,您还需要更改C_VDD和C_VEE电容器比,以与新的电压设置兼容。这些器件基于串联电容分压器、电荷平衡原理、C_VDD*VDD=C_VEE*VEE来调节双输出电压。下表所示的每个变体都有自己的专用Excel设计工具,可从产品文件夹下载。Excel设计工具将显示温度与最大功率限制以及推荐的RLIM、输出电容器比,以获得最佳性能。