This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10987: How to obtain the power of BLDC?

Part Number: DRV10987


I want to know the power of the brushless motor driven by the DRV10987 chip. Currently, my calculation method is to read the value of register 0x04 as the current and the value of register 0x05 as the voltage, multiply these two values and then multiply by 3 to get the power consumption of the motor. However, I saw on the forum that the current in register 0x04 refers to the phase current, not the bus current. So, how can I obtain the total power of the motor through the DRV10987 chip?

The power I calculated based on the above method is around 1.2W, while the total output power of my power supply (control board + pump) is 5.4W. However, when I disconnected the controller from the pump, the static power was 0.7W. 0.7 + 1.2 does not equal 5.4W. Clearly, my calculation method is incorrect.

  • 您好

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待

  • 您好

    I will run bench measurement and provide comparison by tomorrow.

    Usually IDC = (2/3) (Phase current A +B+C), where phase current A is rms value.

    The data sheet is not explaining whether Motor current parameter is rms of all three.

    The accuracy also depends on the lead angle TCtrlAdvShift.

    I have also raised request with design to provide details; I need wait until next week due to holidays.

  • 您好

    The MotorCurrent variable just for indication purpose, this uses limited resolution.

    The internal implementation runs truncation to eliminate the noise and this impacts accuracy.

    Also, phase current should be tuned to well align with BEMF as mentioned before, this improves accuracy little bit.

    Due to the reasons mentioned above, this measurement will have accuracy issues.

    I don't suggest using this variable for any efficiency measurement; please use it only for basic illustrative purposes.