This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8251A: DRV8251,输入信号快速切换电机方向,导致驱动不工作

Part Number: DRV8251A

输入信号原本是 IN1=1,IN2=0,快速切换成IN1=0,IN2=1,设备就无法正常工作,如果在切换的过程中,加入200ms时间的IN1=0,IN2=0,设备就可以正常,请问快速切换方向是否被禁止

  • 您好,

    您可以参考看看查看数据手册11页“8.4.1 Bridge Control ”,电气参数可以看看数据手册第五页,

    https://www.ti.com.cn/cn/lit/ds/symlink/drv8251a.pdf

    When an output changes from driving high to driving low, or driving low to driving high, dead time is automatically inserted to prevent shoot-through. The tDEAD time is the time in the middle when the output is High-Z. If the output pin is measured during tDEAD, the voltage depends on the direction of current. If the current is leaving the pin, the voltage is a diode drop below ground. If the current is entering the pin, the voltage is a diode drop above VM. This diode is the body diode of the high-side or low-side FET. The propagation delay time (tPD) is measured as the time between an input edge to output change. This time accounts for input deglitch time and other internal logic propagation delays. The input deglitch time prevents noise on the input pins from affecting the output state. Additional output slew delay timing accounts for FET turn on or turn off times (tRISE and tFALL).