I haven't connected the MOSFETs and load yet. I want to check the output waveform first, but when I use a symmetric input signal to drive the high-side and low-side inputs of the DRV8328, the measured high-side gate signal and low-side gate signal of the output are inconsistent. The oscilloscope shows a difference. Is this normal? Could it be because I haven't connected the MOSFETs and load?