This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMG3411R150: 一体式1.2KW电机驱动器,LMG3411R150驱动PMSM FAULT异常触发

Part Number: LMG3411R150
Other Parts Discussed in Thread: TIDA-00915

按照官方给的TIDA-00915设计方案,设计的1.2KW驱动电路,目前测试遇到以下几个问题。

整体设计架构:驱动板(六路GaN)-->排针-->控制板(隔离芯片+MCU)

1、低压测试:驱动板功低压48V开环测试电机可以正常运行(程序屏蔽了FAULT信号的输入),FAULT信号一直会叠加干扰信号,将排针上的FAULT信号断开直接测试芯片引脚的FAULT信号已经叠加了干扰信号(干扰信号毛刺测试为控制信号的20KHz)。20KHz的控制信号隔离输出侧无异常。

2、高压测试:DC300V开环测试电机GaN芯片损坏,损坏原因可能是瞬时的直通造成的炸机,原因目前没有分析出来。测试死区时间是600nS。准备先50%的PWM测试高压信号波形是否正常。