This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCF8315C: While use motor studio smart tune, Prompt 'CONTROLLER_FAULT', 'MPET_BEMF_FAULT'

Part Number: MCF8315C

Dear  FAE,

        Prompt 'CONTROLLER_FAULT', 'MPET_BEMF_FAULT',When use motor studio smart tune.
        However motor can spin about 5 second when 'Configuration'

Motor Parameter: 

  Driver Volatge : 24V
  Number of Pole Paris : 1 
  Voltage Constant :   3 mV/Hz
  Resistance Phase to Phase : 2.2 ohm
  Inductance Phase to Phase : 14uH 
  Motor power : < 30W.
  Max Speed:  50000 RPM.
  Application:  Blood pump

   Question:
   1、 How to set parameters the motor can spin?
   2、 can I skip smart tune and write motor parameters to EEPROM directly?

        

 

 

 

  image.png