This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8841: 电机驱动芯片问题

Part Number: DRV8841


该款芯片的pin15是V3P3OUT输出3.3V/1ma,能同时给pin12.13REF参考引脚以及上拉电阻接reset引脚使用吗?REF肯定够用,显示消耗电流6ua,但是reset不太清楚,这个主要是靠外围限流电阻控制的吧?请问上拉电阻多少合适?主要问题是靠PIN15供电的话会出现电压不稳或者导致pin15低于3.3V.

  • 该款芯片的pin15是V3P3OUT输出3.3V/1ma,能同时给pin12.13REF参考引脚以及上拉电阻接reset引脚使用吗?

    是的,有可能。 只要 V3P3OUT 上的电流低于 1mA 就可以了。

    请问上拉电阻多少合适?

    10kΩ 是一个不错的值。

    靠PIN15供电的话会出现电压不稳或者导致pin15低于3.3V.

    只要 V3P3OUT 电流保持在 1mA 以下,就不会有任何不稳定问题。