This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8874-Q1: 电流输出脚IPROPI换算电机电流,实测的结果和换算结果相差较大

Part Number: DRV8874-Q1


按照手册里的电流检测来设计的电路,也是按照对应的公式进行的计算,现在的情况是,实测出来的结果和用公式计算的对应不上。

目前把芯片配成PWM control modeIN2设置为低电平,IN120KHz60%占空比驱动,RIPROPI = 1K,实测VIPROPI = 0.044V,根据公式换算得到电流是97.78mA,但实际电流表检测的电机电流为48.7mA

 实测了从50%~100%PWM驱动下,电机电流和VIPROPI电压,公式换算和实际测到的电流对应不上。

这是什么原因?