3625DWTR芯片 经过多次调试,在PWR VCC+16V,VCC+16V供电脚电压都+16V正常下,把RC-OSC脚电压调到2.0V-3.6V之间时,PDC脚,PDB脚,PDA脚各脚电压都为0V.示波器测也没有波形;PBA脚,PUB脚,PUC脚都有1.7V-3.0V左右的电压。但各脚也都测不到方波形。请查询状况原因。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
通过查看该器件datasheet功能,可以了解到输出(PUA/PUB/PUC、PDA/PDB/PDC)上的输入(H1/H2/H3、DIR)关系如下表所示。 PUA/B/C 用于驱动高侧 PMOS 型 FET、而 PDA/B/C 用于驱动低侧 NMOS 型 FET。
此外,
Input-Output truth table

ISENSE 引脚-涉及过流保护并可触发输出关断: