This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F2800137: Inquiry Using DATALOG Function

Part Number: LAUNCHXL-F2800137
Other Parts Discussed in Thread: C2000WARE, , BOOSTXL-DRV8323RS

from【C2000Ware_MotorControl_SDK_4_02_01_00】

use LAUNCHXL-F2800137 + BOOSTXL-DRV8323RS

CCS 12.1.0.00007

Dear Sir/Ms.

I am currently testing the Level 1~Level 4 Incremental Build project.

When I want to use the [DATALOG module] to display the current current value,

but a lot of errors occur after compiling.

I would like to ask if the error is caused By the fact that the F280013x series does not have the DMA function?

If yes, then I want to use [DATALOG module] on F280013x, how to achieve it?

 

Best Regards,

Yu-Xiang