This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10983: DRV10983的控制启动缓慢问题

Part Number: DRV10983


无刷电机应用

    无刷电机安装有一个风叶,使用DRV10983控制,通过无刷电机在水中旋转,形成反向推力,实现机器运动。目前可以实现速度在600~2500rpm稳定运行,但是启动时间比较慢,需要1500ms。为了使机器快速相应运动,需要将启动时间降低到300ms以内。

 

无刷电机配置
DRV10983
现有配置参数和配置图如下:

 

此配置可以确保无刷电机稳定运行,速度在600~2500rpm.

测试无刷电机相应速度,13:57:44.905 给占空比20%  13:57:46.225才会有速度反馈。启动时间基本都是1500msDRV10983控制启动缓慢说明.docx

提速测试

为了提高无刷电机相应速度,使能了Closed Loop Disable,启动速度从1500ms提高到750ms,DRV10983配置参数和配置图如下:

但是电机的最大运行速度只有1000rpm.