This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCT8316Z: 双电荷泵的工作原理是怎样的

Part Number: MCT8316Z


能说明一下用两个电荷泵进行驱动是什么原理吗

  • 为更加有效地解决您的问题,我需要多一些时间查看这款芯片,稍后会为您解答。

  • 请问您为什么要尝试使用两个电荷泵驱动?需要从驱动程序中获得什么性能?

  • 输出功率级在数据表描述:

    The MCT8316Z device consists of an integrated 100-mΩ (combined high-side and low-side FET's on-state resistance) NMOS FETs connected in a three-phase bridge configuration. A doubler charge pump provides the proper gate-bias voltage to the high-side NMOS FET's across a wide operating-voltage range in addition to providing 100% duty-cycle support. An internal linear regulator provides the gate-bias voltage for the low-side MOSFETs. The device has three VM motor power-supply pins which are to be connected together to the motor-supply voltage.