Part Number: DRV8329AEVM
Other Parts Discussed in Thread: DRV8329, CSD19506KTT, UCC27284, , C2000WARE
半桥栅极驱动器用3个UCC27284替换DRV8329+CSD19506KTT控制BLDC,问题如下:
1、在hal.c中配置PWM, 实测EPWM3无波形,其他两相有PWM波
// GPIO227->EPWM3A->M1_UH
GPIO_setPinConfig(GPIO_227_EPWM3_A);
GPIO_setDirectionMode(227, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(227, GPIO_PIN_TYPE_STD);
// GPIO230->EPWM3B->M1_UL
GPIO_setPinConfig(GPIO_230_EPWM3_B);
GPIO_setDirectionMode(230, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(230, GPIO_PIN_TYPE_STD);
// GPIO0->EPWM1A->M1_VH
GPIO_setPinConfig(GPIO_0_EPWM1_A);
GPIO_setDirectionMode(0, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(0, GPIO_PIN_TYPE_STD);
// GPIO1->EPWM1B->M1_VL
GPIO_setPinConfig(GPIO_1_EPWM1_B);
GPIO_setDirectionMode(1, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(1, GPIO_PIN_TYPE_STD);
// GPIO2->EPWM2_A->M1_WH
GPIO_setPinConfig(GPIO_2_EPWM2_A);
GPIO_setDirectionMode(2, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(2, GPIO_PIN_TYPE_STD);
// GPIO3->EPWM2_B->M1_WL
GPIO_setPinConfig(GPIO_3_EPWM2_B);
GPIO_setDirectionMode(3, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(3, GPIO_PIN_TYPE_STD);
2、参照DRV8329AEVM控制流程,换成非SPI接口的UCC27284,软件怎么移植,能否提供参考文档?
谢谢