您好!
我们在使用 DRV8952来驱动 TEC时,根据应用手册中建议使用低通滤波器。使用的是手册第34页中提到的10μH电感和22μF电容,PWM频率为100K时,我们发现并未对TEC进行控制,且芯片温度很高 。当我们去掉了22μF的电容器后,发现可以进行TEC控制,芯片温度也正常。 您能建议一下使用该部件控制TEC的最佳配置吗?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.