This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8353: 采样电阻滤波的问题

Part Number: DRV8353


工程师,您好。我在用DRV8353H设计电路,想用单电阻采样的方法采样总电流,下面是部分原理图:

R14是我的采样电阻,因为采回来的信号噪声毛刺太多,我计划用R29、R30、C52构造滤波器,我的R29和R30选用10K的电阻,但是这么用会导致SPA引脚的电压超过1V产生过流故障,我不得不采用0Ω的电阻来替代R29和R30,但这样无法滤除毛刺噪声。请问这是因为10K的电阻值选太大了吗?如果我想构造一个10KHz的低通滤波器,R29、R30、C52选取什么值合适?