This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10983-Q1: 调试问题

Part Number: DRV10983-Q1


您好!

有几个问题请问一下:
1,DRV10983Q1 能不能设置PWM工作区间,现在只看到最低占空比设置,低于5%按5%输出,低于1.5%按0输出;有没有最高占空比设置,高于98%占空比按最高速输出?
2,PWM能不能设置对应实际转速,比如我30%占空比对应1000rpm这样的设置?
4,电机启动时间正常是多少,我现在把1阶和2阶加速设置最大,能在8秒内达到目标转速。

多谢!