This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-DRV8323RS: DRV8323RS 驱动无刷电机 电机发热严重

Part Number: BOOSTXL-DRV8323RS


你好,我想咨询下无刷直流电机在三相上加电感来降低驱动电流斜率和幅度,从而降低电机温升的方法是否可行,我们是否有如此的应用。

目前项目是用DRV8323RS驱动三相无刷直流电机,采用六步方波控制,电机电压24V,最大电流4.52A,相电阻:0.245Ω,相电感:30uH。

采用70%占空比驱动,电机温升较高,尝试在电机三相上串电感,温升有降低,三相的驱动电流减小,电流斜率也降低了。

1、想了解是否有次用法,那么电感的选取是否有理论依据

2、是否有其他办法可以降低电机温升

谢谢!