This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV110: Issues related to hold current accuracy

Part Number: DRV110


Hello, according to the specification of the chip, under the condition that the PEAK and HOLD pins are directly connected to GND and RSENSE = 1 ohm, the lower limit of the current deviation is 20%, the upper limit is 30%, and the excitation current is 10%. Please confirm whether the accuracy range of the excitation and holding current that can be set by the chip can be higher.