This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCF8315A: 如何应用在自主开发的板卡上

Part Number: MCF8315A
Other Parts Discussed in Thread: MCF8315EVM

我这边使用MCF8315EVM对性能做过了评估,满足我们的使用要求,现在计划集成于产品的板卡之中,目前有以下疑问:

1> 通过评估板制作好的参数文件,是不是仅通过I2C接口连接就可以将参数配置与EEROM内?

2> 在一个MCU连接两个MCF8315芯片时,有没有办法配置I2C的地址

3> 电路板预留I2C接口是不是就可以实现芯片烧录功能?

  • will lee,您好,

           1 是的,参照“7.6.1.1 EEPROM Write”。

           2 配置“Figure 7-76. DEVICE_CONFIG1 Register” 可更改芯片I2C地址。

              

             注意要执行下面步骤,保证地址被保存在EEPROM中。

             

          3 是的      

  • 针对1个MCU同时控制2个或以上的MCF8315芯片时,如何去设置 Target ID?

  • will lee,您好,

           MCF8315如果没有对EEPROM进行配置的情况下,是采用寄存器内默认地址的。

          对于您的需要,需要您自行进行外部电路设计,比如 对MCF8315进行供电控制等。