This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8706-Q1: DRV8706S-Q1电流采集问题

Part Number: DRV8706-Q1


第一个问题:如图DRV8706S_Q1   第14引脚输出的电压值计算出来电流值是直流有刷电机的瞬时值,可以这样理解吗?

第二问题:第16脚AREF电压是+5V,分流放大器参考电压设置默认AREF/2; 电机停止时SO(14脚)电压是2.5V,电机运行时采集到SO电压为2.75V;此时电机电流为:(2.75-2.5)÷(10*2)÷(5×10-³)=2.5A 这样计算电流值算法正确吗?此时电流表显示的电流值约1.5A。造成这个差异是什么原因?有没有精准的算法。