我在设计电机驱动器的时候参考了 SLVA835A利用DRV8323RS的VCP引脚串联一个电阻接到NMOS的G级,电源供电是24V,现在可以测到VCP引脚是35.3V,但是经过电阻到NMOS的G级以后只有24.25V了,没法打开NMOS,可能是什么原因导致的呢?NMOS使用的是 NCE60H10K
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在设计电机驱动器的时候参考了 SLVA835A利用DRV8323RS的VCP引脚串联一个电阻接到NMOS的G级,电源供电是24V,现在可以测到VCP引脚是35.3V,但是经过电阻到NMOS的G级以后只有24.25V了,没法打开NMOS,可能是什么原因导致的呢?NMOS使用的是 NCE60H10K
您好,
您图示的器件未焊接吗?完整的电路如链接内文档Figure 6所示,
如果不想使用BJT,可参考Figure 3电路。
Protecting Automotive Motor Drive Systems from Reverse Polarity Conditions (Rev. A)