This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8353: DRV8353的SOA等波形异常

Part Number: DRV8353


尊敬的TI专家们,您好:

我在使用DRV8353SR时遇到以下两个问题

1.在PWM未输入的情况下,通过给芯片EN信号,抓取到在使能信号后16us左右,fault引脚有一个跌落,芯片报0x700错误,我通过抓取三相的VGS电压,均未有异常开启情况,但报此错误后输入PWM,三相PWM均能正常输出,请问此fault跌落是什么问题,会否对使用造成影响? 下图中通道1是EN引脚信号,通道3是fault引脚信号

2.我们在未接电机的情况下,三相PWM输出50%占空比,我们的ref电压时3.3V,测试三相SOA/B/C电压时,发现在相电压上升前1us左右,SOA/B/C等电压均下降到0 ,且每个周期均会出现。测试三相采样电阻上电压,同一时刻均没有电压波动,后抓取VGLS,DVDD电平均比较平稳,请问此问题可能是什么问题?该从哪里进行排查?谢谢

下图中通道1是SOA信号,通道3是SOA信号