This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8353: DRV8353 drive waveform testing

Part Number: DRV8353


DRV8353 drive waveform testing

48V, PWM 20KHZ, dual mosfet, sink 600ma,source 400ma , Dead-time200ns

The schematic diagram is as follows

1-channel (yellow) GHC-SHC, upper bridge VGS voltage

2-channel (green) SHC, phase voltage

3-channel (blue) GLC, lower bridge VGS voltage

 

 

The lower bridge VGS has oscillations with a significant amplitude, and the upper bridge also experiences voltage rise. Is it reasonable or does it have hidden dangers. I tried to suppress the amplitude of the oscillation:

 

1100K resistors are connected in parallel between VGS, without significant changes

2Reduce the driving current, sink 300ma  source 300ma ,The falling edge slows down, but the shaking still exists, and the shaking amplitude should be lower 

3Increase the driving current, sink 800ma  source 550ma ,The edge shakes more, but the shaking still increases

4The driving current remains unchanged (sink 600mA source 400mA), and without 100pF between GS and 100K pull-down resistor, the oscillation increases slightly

5Adjust the driving current (sink 600mA source 300mA) and add 100pF. Without 100K pull-down, the oscillation increases slightly ,Is this OK?