This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
按照DRV2700使用手册进行模拟信号的放大,电路参考使用手册进行设计,预期BST为100V,并在OUT+端出现放大后的正弦信号,[gain1,gain0]=[1,1]。在输入信号为空时,OUT+与OUT-端都出现330HZ左右的方波,峰值为BST的一半。在输入正弦信号时(由开发板DAC输出的峰值为3.3V,偏置为1.15V,也即正弦波的最低值为0),输出结果为一段一段的方波,方波最大幅值与正弦波的采样一致,并不是连续的正弦波。已经测试三个电路,都是一样的结果。电感使用了最大电流为1A,电感值为6.4uH的功率电感
电路原理图:
输入信号为空时,OUT+与OUT-端波形:
输入正弦信号时,输出波形: