Part Number: MCF8315EVM
Other Parts Discussed in Thread: MCF8315C-Q1, MCF8315C
使用外部时钟并没有改善时钟精度,反而在8kHz等频率下出现频率震荡,感觉像锁相环没锁住一样,外部时钟使用信号发生器生成0到3V,50%占空比的方波
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MCF8315EVM
Other Parts Discussed in Thread: MCF8315C-Q1, MCF8315C
使用外部时钟并没有改善时钟精度,反而在8kHz等频率下出现频率震荡,感觉像锁相环没锁住一样,外部时钟使用信号发生器生成0到3V,50%占空比的方波
I have send a video on bilibili https://b23.tv/s5Dg1De,when I use a 64kHz external clock, the FG was always moving, And if i use the internal osc, then the moving is better. what is the wrong, by the way, Can I use the MCF8315C-Q1 as a current loop controller which can input both positive and negtive Iq curr Ref, and build a speed PI outside the MCF8315C using a MCU, to imporve the speed accuracy。 I think is better to have a choose to put a 16Mhz CRYSTAL XTAL with this MCF,and like a c2000 dsp, or we build c2000 in the MCF
I have read these two questions ,they are no helpful , but they didn't answer my question , I use a external clock, it change worse compare with internal, how can we know the clock accuracy is improved by the external clock,Can we confirm this by observing the signal like the SW_BK PIN,FG,OUTA,OUTB,OUTC.
Can you arrange someone chinese person help me to solve problems on site,my phone is +8618911988392
您好,
请确认一下下面的回复:
要使用外部时钟,我们需要遵循下面列出的步骤,请确认您是否遵循此步骤
1.启动时设备在内部振荡器上运行
2.设置外部时钟与正确的频率,我们将在接下来配置
2.1示例:如果您要应用64KHZ,则准备64KHz源并应用于EXT_CLK引脚
2.2写入DEVICE_CONFIG2[EXT_CLK_CONFG]= 64KHz
2.3写入DEVICE_CONFIG2[CLK_SEL]=外部时钟输入
3. WRITE DEVICE_CONFIG2[EXT_CLK_EN]=启用
如果启用了外部时钟(步骤3),则在应用时钟或使用正确的时钟设备将其配置为正确的值之前,将重置并切换回内部振荡器。
请确认上述流程,如果未完成,请尝试重新检查行为。
关于IQ控制,是的,MCF8315C可配置为扭矩模式(当前模式)并控制IQ方向,从而控制方向。 但内部速度回路精确度在温度范围内高达3%,如果使用外部时钟,我们应该期望更好的精确度。
您好,
1、首先,我就是按照这个步骤操作的,确实没什么改善;
2、我知道可以设置位扭矩模式,我问的问题是在同一时刻,即可以让Iq_ref为正,也可以为负,“Can I use the MCF8315C-Q1 as a current loop controller which can input both positive and negtive Iq curr Ref”,如图所示,比如50%占空比电流为0,小于百分之50%电流为+,大于百分之50%电流为负。您说的控制"并控制IQ方向,从而控制方向"这个方向怎么控制?