This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
对于DRV8412来说,其datasheet中对于TEC的驱动给出了图 7-10. Application Diagram Example for TEC Driver Schematic。这里需要4个LC滤波网络。但是在并联全桥模式(1 PFB)时,OUT_A和OUT_B内部是同步的,假设四个半桥的功率级电源都是同一电源,那么是否A\B这一组两个半桥输出可以共用一个LC滤波网络,C\D同理。实现与DRV8262类似用2个LC网络来驱动TEC的效果,进一步地节省PCB面积?
您好
对于DRV8412在并联全桥模式下LC滤波网络的使用
一、DRV8412并联全桥模式简介
DRV8412是一款高性能、集成式的双全桥电机驱动器,支持并联全桥模式(1 PFB),在该模式下,OUT_A和OUT_B内部是同步的,可以实现对电机的双向控制或驱动更大的电流。
二、LC滤波网络的作用
在驱动TEC(热电冷却器)等负载时,LC滤波网络用于平滑输出电流,减少纹波,提高驱动效果。
三、并联全桥模式下的LC滤波网络使用
1. 共用LC滤波网络的可行性
2. 注意事项
四、结论
在DRV8412的并联全桥模式下,若满足一定条件,A\B和C\D两组半桥输出可以分别共用一个LC滤波网络,实现与DRV8262类似用2个LC网络来驱动TEC的效果,进一步节省PCB面积。但具体应用时需注意滤波网络的设计和测试验证。