This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DRV8908-Q1可以接内阻为2-10Ω的感性负载吗?我们将一个半桥输出PWM,然后接振子(内阻为2-10Ω的感性负载),另外一端接电源或者地都报错,会报过流或者欠压,这个驱动芯片是不是只能接内阻很大的负载?
您好
这个内阻确实比较小,8908手册里面给的例子是大于10Ω的。
我也看了其他芯片,8806给的数据也是16Ω,但是电机绕组电阻RL给的是7.4 Ω/phase,您可以看看,目前没有看到其他更小的。
所以说感性负载最好都是10Ω以上的,电机的话7.5Ω以上的?
这是用的半桥PWM驱动的小电阻感性负载,一端接PWM out,一端接电源或者地,所以会检测到过流和欠压。
但是如果小电阻感性负载两端接两个半桥可以正常工作吗?