Part Number: DRV10970
之前我提问有毛病,今天重新问一下。
我选用的是直流无刷电机,内置3霍尔传感器数字输出,3霍尔传感器的摆放角度是60°。
DRV10970的“CMTMOD”引脚,可以配置3种模式,但不包括对应60°摆放霍尔传感器的情况,所以,是不是DRV10970无法用于驱动此电机?如果是的话,是否知道合适的型号,请推荐。谢谢!

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.