This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCT8316AEVM: IIC写数据成功,但是掉电不保存

Part Number: MCT8316AEVM
Other Parts Discussed in Thread: MCT8316A,

当我们使用MCT8316A这款芯片以及TI 自己的MCT8316AEVM这款开发板时,IIC通讯往芯片写数据可以写进去,但是掉电以后无法保存,我们已经很多次遇到这问题,希望TI的支持可以协助我们解决这一问题,谢谢!

When we use the chip MCT8316A and TI's own development board MCT8316AEVM, IIC communication can write data into the chip, but it can't be saved after power failure. We have encountered this problem many times. I hope TI's support can help us solve this problem. Thank you!

  • 您好,

         我看到FAST_DECEL_EN设置

        如果您打算测试 FAST_DECEL_EN能否 DYNAMIC_BRK_CURR 设置为 0b 告诉我们FAST_DECEL_CURR_LIM是否有效

         另外 FAST_DECEL_CURR_LIM 不起作用您的意思是消耗电流得多如果您如何测量电流