This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8662: 啟動順序,先EN再Vdd會有問題嗎?

Part Number: DRV8662

Rext : 6.98k ohm,L:4.7uH

Boost電壓至105V,無接負載狀況下,Vdd送電之後再EN to high,順利啟動輸出至105V,

但是EN如果先在high的狀態,Vdd才送5V,則電壓上升不到105V,Vdd反覆on off,則DRV8662冒煙燒毀。

啟動順序一定要先Vdd再Enable嗎? boost的電感飽和嗎?  還是其他問題造成的?