Other Parts Discussed in Thread: LM5158, TPS61391
Hi ,
我有个案子,需要产生一个很高的电压(80~90V)用来驱动压电风扇(功率不大,小于0.5W),供电源是单节锂离子电池(3~4.4V,下截止电压可以上浮)。
我看到TI这边有TPS61391和LM5158都可以升压到这么高的电压。我不太确定,请问这两颗料是否都合适我的需求?两者在应用上有什么差异?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这两个芯片都能升到80V,下面是两者主要参数区别对比:
建议可以参考WEBENCH辅助设计: