使用BQ24617作为充电管理芯片,
输入电压:10.8-12.6V
电池端:2节18650锂电池并联(7.2-8.4V)
问题:当AC adapter供电给BQ24617,不接电池的时候,SYSTEM路径(原理图中的BAT_VSYS)没法获取稳定的输出电压,会脉冲一段时间后,直接没有输出。当有接电池的时候,SYSTEM路径需要几秒钟才能获得稳定的电压,BATDRV信号有脉冲,请教为什么?怎么样才能获取稳定的SYSTEM电压,不管电池存在不存在?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用BQ24617作为充电管理芯片,
输入电压:10.8-12.6V
电池端:2节18650锂电池并联(7.2-8.4V)
问题:当AC adapter供电给BQ24617,不接电池的时候,SYSTEM路径(原理图中的BAT_VSYS)没法获取稳定的输出电压,会脉冲一段时间后,直接没有输出。当有接电池的时候,SYSTEM路径需要几秒钟才能获得稳定的电压,BATDRV信号有脉冲,请教为什么?怎么样才能获取稳定的SYSTEM电压,不管电池存在不存在?

不是,现在现象是这样子的:
不接电池的时候,只有AC端输入,那么SYSTEM端的输出一直是脉冲波形;
当接了电池(2S,7.2-8.4V),又有AC(10.8-12.6V)输入,SYSTEM的波形是周期性的在AC电压和8.4V左右切换;
另外我发现ACDRV信号一直到不了规格书里面说的VCC-6V,不管是AC输入存在或不存在,都始终到不了VCC-6V,我觉得因为这个问题,所以导致BATDRV一直处于一会导通一会关断的状态,帮忙分析下?多谢
BR
jw
有没有可能用PG这种信号替代BATDRV,只要AC输入端有电压,就直接使用AC输入?另外ACDRV的VCC-6V能再哪里可以测量到吗?
BAT_VSYS断断续续,说明Q25或Q9,时开时关。可以看下这两个管子的驱动信号,看看哪个不正常。然后,进一步查找出驱动异常的来源。